Other Parts Discussed in Thread: CSD18543Q3A, TPS43061
Hi,
I've developed a circuit to boost the input from 12V to 30 V using TPS43060 (I did use Ti WebBench for that).
The problem is that there is not switching frequency generated form the device, therefore, It cannot drive the gates of the two Fets (CSD18543Q3A). I've built three different circuits to compare but they have the same problem; no switching frequency. I've also followed the configuration from the evaluation board but there was no difference, and there was 7.5V at PGOOD pin.
What could be the sources of the problem?
Thanks in advance.
Regards,
Nghia