Hi Expert,
I have a request of TPS74801 application need you help to double check.
Customer spec, Vin= Vbias=3.3V, Vout = 1.8V and Iout=0.06A.
From datasheet recommend the Vbias need large than Vout+1.6V, and test condition at 1.5A output.
But check the customer spec, the output current only 0.06A.
So do you have any concern to the customer design? do you approve this design under very light load condition?
Due to customer will tape out tomorrow, so please help to feedback ASAP.
Regards,
Mark