hello.
I made a circuit (Attachment 1) with reference to the recommended circuit in the data sheet and confirmed the operation, but the problem was that the output dropped and became unstable under a load of several mA.
I suspected a malfunction of the overload control, but in the no-load state, noise occurred on the CS pin and the output did not drop even if it exceeded the overcurrent threshold of 0.1V.
I have attached the created circuit (Attachment 1), so can you tell me if there are inappropriate parts in the constants, etc.
Also, I think that this problem is caused by the CS pin, but please let me know if there are any precautions (part layout, constants, etc.) regarding the CS pin.
Most ICs have a blanking time on the CS pin. Is there a blanking time on the CS pin of the LM5155?