Hi
We are considering to use BQ25155 battery charger IC in our design to charge a single cell Lithum polimer battery. In the data sheet I have studied about VIO pin. Instead of connecting this PIN to IO power lines of our system, we want to connect it to an GPIO PIN of CC2642 which is a BLE simplex device of TI. Connecting to GPIO will give us power advantage we believe(we can turn it off or on as we prefer to control the usage). GPIOs can provide up to 8mA in Extended-Current(EC) mode. I have following questions in this regard.
A) What is the max current drawn by VIO?(could not spot it in data sheet absolute max ratings, probably I am missing something here)
B) Can we think in those line of connecting GPIO to power the VIO? If yes please give us some application note to support the said design.
B.1) This device is also having an interrupt to inform faulty conditions. If we power it using I/O then if there was a faulty condition (which has occurred at the time of no-power to VIO) will the interrupt and other digital-status be made available at the time of bringing back power through GPIO?
Regards,
Pothirajan.K