This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] BQ25150: BQ25150 and BQ25155 Differences

Genius 17745 points

Replies: 0

Views: 24

Part Number: BQ25150

Feature BQ25150 BQ25155
PMID Regulation Not supported. VIN is pass-through to PMID PMID is regulated and can be programmed through I2C. Default voltage is 4.5V
VINDPM Enabled at 4.6V default Disabled by Default
IMAX Supported Not supported (Reduces BOM by 1 resistor)
Default Input Current Limit 100mA 500mA
Minimum PMID Capacitance 1uF 10uF for PMID regulation
Shipmode wake Timer for /MR 2s (wake timer 2) 125ms (wake timer 1)

Regards,

Sharafadeen Raheem

Applications Engineer

Battery Chargers

Please click "This resolved my issue" button if this post answers your question.

Check out TI’s new Advanced Linear Charger with 16-bit ADC & LDO

http://www.ti.com/product/BQ25155