Hi Team,
What is the overcurrent value (Maximum) of TPS65910A3A1RSL?
Thanks,
Taishi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
What is the overcurrent value (Maximum) of TPS65910A3A1RSL?
Thanks,
Taishi
The TPS65910 has 4 DC-DC converters and 8 LDOs integrated. Many of them will have different over-current values.
Some of the regulators also have configurable maximum load currents.
For example, VIO (DC-DC converter) has PMOS current limit (high-side) configurable by ILMAX[1:0] bits. When ILMAX[1:0] = 10, the guaranteed minimum current limit is 1700mA. All devices will allow up to 1700mA (minimum guaranteed value), but the current will be limited at a slightly higher threshold. It is a minimum spec for a maximum value.
VIO also has NMOS current limit (low-side). VDD1 and VDD2 have the same PMOS current limit (high-side) and NMOS current limit (low-side) specifications but are only configurable by 1 ILMAX bit (0b or 1b).
The LDOs are specific with a different value, named "Load current limitation (short-circuit protection)" that has a guaranteed minimum value and typical value listed for each LDO.