The TPS50601-SP datasheet has the typical and maximum value for the minimum on time but only a typical value for the minimum off time. Can it be assumed that percentage tolerance of the minimum off time is the same as the percentage tolerance of the minimum on time?
For example, the typical and maximum values of the minimum on time are 94 ns and 175 ns, respectively, and using that assumption the maximum value of the minimum off time would be 431 ns.