Part Number: LM74700-Q1
The LM74700-Q1 datasheet lists its "enable input high threshold" as 1.06V (min), 2V (typ), 2.6V (max), which is a curiously (and, for me, inconveniently) big range (well over a factor of 2 from Vmin to Vmax!). I have an application where I will, for a short while (when starting up the MOSFET), be driving this enable pin with a 3V ML1220 rechargeable coin cell, which actually spends most of its operational life at 2.5V +/- 0.1V (see page 4 of https://media.digikey.com/pdf/Data%20Sheets/Panasonic%20Inustrial/ML_Serie.pdf). Let's say that I can guarantee the ML1220 will be at least half-charged, so I can provide at least 2.4V to the enable pin (but maybe not 2.6V).
Will the LM74700-Q1 possibly not turn on if I only provide 2.4V to it? Does the 1.06V (min), 2V (typ), 2.6V (max) range represent part-to-part variation? I can't imagine your ICs would vary that much. I imagine that the enable pin is connected to the gate of a transistor at where it comes onto the LM74700-Q1. I suppose I could pipe my enable signal (powered by the ML1220, at 2.4V or higher) into another transistor, and use the output of that to drive the enable input of the LM74700-Q1, but that really seems redundant.
So, my question: will 2.4V or higher provided on the enable pin of a LM74700-Q1 reliably enable the MOSFET to which it is connected?
Thanks in advance for the clarification,
Tom