Hello team,
1. Feedback resistor.
In the datasheet, Vout is determined by 0.768*(1+R1/R2).
Although customer calculate the R1 with R2 = 10kohm, they found the gap between the calculation value of 32.97k ohm and the recommendation value of 33.2k ohm.
Which should customer follow ?
2. Peak current and RMS current
Customer calculated the value of peak current and the RMS current using equation 4, 5, 6 with table1. Design parameters but they found out that there is mismatch between calculation result and the description in the datasheet.
Is it typo ?
Thank you and best regards,
Michiaki