This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 3
Views: 58
Part Number: TPS61196
Hi Team,
We got a question from our customer regarding abnormal phenomenon.
The phenomenon is that the anode voltage rise up to OVP point when the dimming duty is changed from 20% to 99.8% quickly. (then LED is light off because of OVP = 58.3V.)
The condition is ;
Vin=12V, 4 LED strings (Unused 2 strings are connected to ground.)
The phenomenon appears;
1.) when the dimming duty is changed from 20% to 99.8% quickly.
The phenomenon DOES NOT appear;
1.) when the dimming duty is changed slowly.(20% to 99.8%)
2.) when the LED strings are reduced to 3. (4strings to 3strings)
3.) when Vin is over 12.5V.
4.) when the dimming duty is fixed 99.8%.
At the beginning of question, we suspected not enough the performance of load transient. So, we asked them to change the compensation circuit at COMP pin or to add Cff.
However those were no effected.
I am at a standstill on this issue. What should I check any other point ?
(Would you mind if you check the schematics on private message? The schematic of their board is confidential information.)
Best Regards,
Koji Hamamoto
Hi Koji,
Yes, you can send me the schematic through the Email. There are a few things that I want to check:
1. What's the LED forward voltage range for the whole current range?
2. Have you observed the Vin waveform when you quickly change the Duty from 20% to 99.8%, it may trigger UVLO?
BR
Sean
In reply to Sean Zhou:
Hi Sean,
Thank you for your support as always.
We had contacted each other about TPS61196 as well before. So, I will send some information by e-mail.
Regards,
In reply to K.Hamamoto:
Sure, Let' talk about this off-line.