Hello,
This is Anurag and I am working as a design engineer in 6th energy technologies. I started working with TPS61022 IC for my application. I am providing my input voltage as 3.8V and my feedback resistors are R1 =100K and R2 =680K and I am expecting my output around 4.6V. Inductor I am using in the circuit is 1UH ,9A. All other passive components are connected as per the datasheet.
After powering on it started behaving normally with out load,but once after connecting the load of around 3A, it started behaving like a buffer. So, can you please help me out in solving the issue.
Thanks and Regards,
Anurag P
9008684764
Email : pullabhotla_anuraag@yahoo.com