Hello Team
I would like to know if you have more information and tests in regard to the maximum current level that the driver could work at the same time for each channel? I am interested to use some RGBs that are available to work up to 150mA, then, I was considering to connect two channels for each LED.
I've seen that the datasheet talks about RGBA, I was wondering if it doesn't have any problem if I want to work just with RGB colors? is it possible to use the other free channel for another color? i.e. Ambar output?
If you have another device that could work with this current level, please, let me know.
Thanks!