Hello,
Does the LM3880 have the ability to change the delays between flag events? I see the datasheet, on Table 1, says the flag timing delay is set at 30 ms. Is this time adjustable at all (without having the factory have to re-program the EPROM)? I was hoping to get it between 5-10 ms per flag event.
If the LM3880 does not have this option, is there an alternate part? Also, is there a part comparable to the LM3880 that has 5-6 channels?
Thanks,
Zach