Hi team,
My customer is evaluating the LM5160EVM with an inverting circuit configuration. The customer connects VOUT and GND in reverse to get an inverted output voltage.
Condition : Vin=+12V~+48V, Vout=-5V, Iout=~2A
The customer mentioned that the Vout ripple was observed around 100mVpp at the constant output current. The customer would like to reduce the ripple voltage. Could you tell me how to reduce the ripple voltage, and how much can the ripple voltage be lowered?(e.g. 10mVpp)
The customer uses Type2 configuration, so they added Cff between the FB and Vout. R3(R8 on the EVM) is still 0.47ohm. According to the equation(7), should customer increase the R3 value to reduce the ripple voltage? In that case, customer need to care load transient response because R3 affects to the load transient response?
Regards,
Yamaguchi