This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61046: tiny package and tiny Iq solution

Part Number: TPS61046

Hi Team,

I would like to find the solution which meet below requirement . I find TPS61046 in ti.com. Do we have more appropriate solution? or next gen roadmap could send me directly?

Description

Vin

Vout

Iout

Efficiency @12V, 10mA

Iq (typ., no switching)

Isd (typ.)

Dimension

15V Boost

3-4.5V

14-16V

>50mA

>75%

<300uA

<300nA

<1.5mm^2

Regards,

Roy