Hi,
Can we add an RC delay (36kohm/0.22uF) @ ON1 pin? Any side effect?
Thanks!
Antony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can we add an RC delay (36kohm/0.22uF) @ ON1 pin? Any side effect?
Thanks!
Antony
Hi Antony,
Welcome to E2E!
An RC delay may be connected to the ON-pins of the TPS22976. The ON-pin of the TPS22976 has a hysteresis of 90mV. Once the device is turned ON, due to the hysteresis, the voltage on the ON-pin would have to drop 90mV for the device to turn off. As long as there's no voltage fluctuations on the voltage of the charging capacitor that exceed the hysteresis, the device will remain ON.
The ON-pin should still not be kept floating. If the enable signal that's going to be used can actively pull the node to ground or 0V, then no additional components will be required. If the signal is left floating in the disabled state, then you will have to add a resistor in parallel with the capacitor(i.e. connected from ON1-pin to GND) to ground the ON-pin in the disabled state.
Best regards,
Andy Robles