Hi,
For BQ25155, VOL value under test condition of Load current of 5mA is (0.25 * VIO) V.
If my load current is much lower than 5mA, does this also mean that the VOL of BQ25155 is lower than (0.25 * VIO) as well?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
For BQ25155, VOL value under test condition of Load current of 5mA is (0.25 * VIO) V.
If my load current is much lower than 5mA, does this also mean that the VOL of BQ25155 is lower than (0.25 * VIO) as well?
Thanks
Hi,
I have MCU GPIO that interpret LOW state at maximum voltage (VIL) of 0.42V. Then, I2C maximum LOW state output voltage (VOL) for BQ25155 is 0.525V (0.25*2.1V). VIO of the charging chip is 2.1V.
MCU GPIO might not interpret as LOW because input signal to GPIO is higher than 0.42V.
Any solution to this?
Please advise.
Thanks