Part Number: UCC28070
Hi,
I would like to ask a question about the UCC28070 device.
I am creating a board and checking the operation of the board.
The measurement waveform is attached.
It operates normally with a load of 4A, but if the load current value is lowered to 1A, the current value of the B side channel decreases.
When the output current decreases, does the current value supplied to the A and B channels become uneven?
Is this behavior normal?
Best regards,