Part Number: LM2576
Dear Sirs or Madams,
Will LM2576 be damaged if reverse voltage is applied to OUTPUT pin(Pin2)?
Here, "reverse voltage" means the condition that the voltage higher than the vltage on VIN pin(Pin1) is applied to OUTPUT pin(Pin2).
For example, what will happen if 15V is applied to VIN pin(Pin1) but 24V is short-circuited to OUTPUT pin(Pin2) by mistake?
Is there the possibility that LM2576 is damaged?
Best regards,
Shinsuke Tanaka