This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62740: LOAD Pin

Part Number: TPS62740

Hi everyone,

I will use the TPS62740 in one of my designs. I will utilize the LOAD pin to supply some of the analog and digital components such as Voltage reference, Op Amp, Multiplexer, Flah memory etc.

So I have to use both AVdd and DVdd lines. I will split the LOAD pin output to create these voltage rails as shown below

My questions are:

1. Is this approach correct for creating AVdd and DVdd?

2. I have to decouple both legs or could I decouple right next the LOAD pin? Should I use the same RL filter provided at the datasheet (decoupling the Vout)?

Thanks in advance

Nick