Other Parts Discussed in Thread: UCC27712
I designed the circuit with the combination of UCC28780 and UCC27712D.
I would like to have a specification that shuts down the main power supply when an abnormality occurs on the secondary side. As a way of realizing it, first get the status from the photocoupler and use it together with a latch circuit (such as a one-shot multivibrator) to completely stop the operation of the UCC28780.
I am worried about the processing method after this.
I am wondering which pin should be used to shut down. The UCC27712 does not have an ENABLE pin, so it seems difficult to shut down.
So I'm thinking of using NTC (9pin).
I'm thinking of preparing a 10kΩ resistor in parallel with the NTC thermistor and forcibly setting it to 10kΩ or less in the event of an abnormality.
Is there a more practical way?
If I force the RUN pin LOW, it won't shut down, right?
If it can be realized with the RUN terminal, it may be better.
B.R. Tak