Hi team.
Can I use at my conditions?
Vin=5V
Vout=±5V
Sincerely.
Kengo.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kengo,
I have notified our expert regarding this topic. Please expect a response by 6/18/20.
Thanks,
Aaron
Hello,
Per the datasheet specification, VPOS regulated range is from Vin+0.5V - 15V.
So with Vin of 5.0V, minimum VPOS needs to be 5.5V. Since Vin is already 5V, you could simply use Vin for your +5V requirement.
For the inverting buck-boost converter, generating VNEG=-5V from Vin=5V is not a problem.
Kind Regards,
Liaqat