Other Parts Discussed in Thread: LM317-N,
Hi,
In one of our projects we are using LM317-N for converting 27V to 5V @ 50mA, in field after running for sevaral months the regualtor is faling(getting short).
Input : 27V
Output: 5V
Current: 50mA
power dissipation: 1.1W
Please review the layout attached, is the copper plane given for thermal dissipation(Vout) is enough?
- plane in orange is the vout plane(copper thinkness:- 0.5 oz.).
- components in red are the feed back circut.
- yellow is the input capacitor
- blue is the output cap.