This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430: schematic check --negative output

Part Number: TPS5430
Other Parts Discussed in Thread: LM337

Dear team,

When configure TPS5340 as a buck boost, the TPS5340 can output negative value. TPS5340's output is LM337's input. When disconnecting these two device, they are working normally, but once connecting these two device(LM337 has no load at this time), TPS5340 will be damaged.  Is there any wrong with the TPS5340's design? Could you please help analyze this question? TPS5340's input is smaller than 30V.

Thanks & Best Regards,

Sherry