Hi,
I use TPS61099 to boost a minimum 3.4V (VCC) supply from Li-SOCL2 battery to 4.3V/15mA, in order to maximize life of battery and reduce ripple voltage of VCC as small as possible, I want to have smaller input and output ripple voltage.
From DS of TPS61099, 2.2uH inductor is fixed to have better stability performance, so I can't use larger inductor to get that, only have one more bulk capacitor just as what WEBENCH gives.
1% output ripple voltage, is it possible to implement with only adding one more 150uF bulk capacitor with low ESR?
My current design has about 1.2mA input ripple current and about 2% ~ 2.5% * 4.3V output ripple voltage.
Or any other good practices can be taken to get smaller input ripple voltage/current to extend battery life.
Thanks.
Regards,
Ma Dawei