Other Parts Discussed in Thread: BQSTUDIO, BQ40Z50
Hi
I completed running cycle charging up to 100%, but the Update status did not change to 0x05. (FC value flagged)
Bit Registers is Update Status=0x04, FC=1, QEN=1, VOK=0, RDIS=0, REST=1
My cell specification is nomal voltage= 3.85v, max voltage= 4.4V, cut off voltage= 3.0V, 2910mAh, 11.2Wh and I am using 3 cells serial.
I received the GPC_report ( Best chemical ID:1181 Best chemical ID max, deviation, % : 3.12)
And I chose a COSLIGHT CA555070(2270mAh) 1181 LiCoO2/carbon3-4 program selected
Design Capacity mAh = 2910mAh
Design Capacity cWh = 3361 cWh (2910mAh x 3 serial x 3.85V / 10)
Design Voltage = 11550mV (3.85V x 3 cell)
What am i doing wrong?