This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP38692: Dropout voltage at 0.5V

Part Number: LP38692

Hi expert,

Customer has two questions:

1. What is the Dropout voltage (Vdo) (Typ) (mV) 250 test condition?

2. When Input id 5.5V, output voltage is 5V, and current is 0.5A, what is the typical  and max dropout voltage?