Part Number: BQ76930
Hi
My customer test with BQ76930 and find a query as below.
The BQ76930 experienced a problem in the discharge of heavy load, the balance circuit has a weak open state on the balanced circuit. After analysis, the problem is as follows:
1. Under heavy load, battery voltage drops, the capacitance between the BQ chip BAT-VC10X, VC10X-VC5X, and VC5X-VSS will be discharged by sampling the input resistance to the battery
2. A voltage drop of about 50mV on the input resistance Rf. The voltage drop is related to the size of the capacitor. Since the balanced MOS uses a low-voltage NMOS, the 50mV voltage drop between gs will make the MOS have a weak current.
Want to know if there is any solution to solve this problem.
Thanks
Star