Hi Team,
Good day.
My customer is working with LM1117IDT-5.0 and wanted to clarification on the worst-case VOut performance with respect to temperature. Checking with section 7.6, page 8. of datasheet Vout is specified as 4.8 to 5.2 V over a -40C to +125C range. On-Page 9, Temperature Stability is specified as 0.5% and Long Term Stability as 0.3%. On page 10, Figure 6 Typical Temperature Stability is shown to be perhaps +/- 0.25% from -50C to +150C.
Can you share with us what is the correct interpretation of the Temperature Stability is specified as 0.5% and Long Term Stability as 0.3%? is that error? Is this exclusive or inclusive of the 4.8 to 5.2 V range specified under VOut?
Thanks in advance.
Renan