Part Number: TPS76901-HT
Other Parts Discussed in Thread: TPS7A8300,
Hello,
I was wondering if the bare die package allows for the reference voltage to be set by wirebond configurations. I have seen voltage regulators for which the reference voltage is set by a bias current fed into a resistor chain. And these parts would have bond pads connected at different points along this resistor chain that would allow the user to change the voltage reference bias resistor's resistance (thus voltage) by connecting to ground. Is there access on the die to to do this, or does the reference bias topology even allow for this? The figure below illustrates what I mean about configuring the reference via wirebonding. For example, If I wanted to have a 3.3V output, I would tie the feedback and output together and connect the 3.3V_REF node to ground. I could also connect the 1.8V_REF node to ground to easily get a 1.8V output. I hope this makes sense.
Regards,
Brandon