I want a simple FET driver to connect between a diode bridge and bulk filter capacitance. The bridge output will be 0 to about 25VDC (bus voltage) and it will switch at around 120 Hz. I'd like to use the LM5050 but I need the FET to deliver current in both directions (in and out of the cap) - could I connect the LM5050 "In" and "Out" pins together to disable the diode mimic function of the part? The FET would only connect to the "Gate" and "In" pins of the LM5050.
If this is not possible, can you suggest an alternative configuration, or an alternative part. Some of the half bridge drivers have under voltage lock out so not suitable - I need the FET to turn on with little or no bus voltage.
David