I am struggling to get this chip to output the necessary voltages to drive the CHG and DSG FETs. I have been playing around with the bq28z610EVM and measuring the voltage at the pins results in a roughly 17.9V output when the FET_EN command is sent to the device. When working with the BQ chip on our custom hardware, the DSG voltage never gets above 2.5V and the CHG pin seems to always be sitting at 8.2V (which in this case is our input battery voltage). I've gone through the settings quite a few times and I'm running out of places to look. Just curious if anyone else has had issues with the FET drive on this part.