Hi,
I'm using LM5140-Q1 QuickStart tools Rev A2, I have a discrepancy between the Inductor value suggested using the tool and the datasheet formula (12): recommended value in the tool is 1.4uH and a comment in red states "Do not chose inductance greater than twice...", I used a 1.8uH 10mohm inductor, the ripple current (row 30) is 56%. Using datasheet formula (12) with Vout = 3.7V , FSW = 440KHz and Iout = 7.5A the inductor value should be more than 3.7uH (ripple current 30%) or 2uH (using 56% as ripple current). If I'm using the suggested value of 1.4uH I'm not respecting formula (12) , but if I use a 4uH I'm picking a value than is more than twice the suggested one... What I'm missing?
Regards
Fabio