Part Number: BQ25895
Hi,
We're finishing a design based on the BQ25895, with QuickCharge inputs (12V 1.5A). However, after doing EMC testing we noticed we're over the maximum allowed limit for the FCC certification, specially around 150 to 250 MHz.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The EMI could be sourcing from:
1.Cables with length 0.3 to 0.7m range radiation in the range
2. Damped SW ringing, either from the ringing or the falling edge.
The following actions may be helpful:
1.Add 1nF PMID, SYS, VBUS (opt.), BAT (opt.)
Recommend X7R 1nF (0402) which typically has > 300M resonant frequency. Please check with vendor for impedance response.
The cap on PMID with minimal loop with IC is the top priority.
2.Slower SW node switching slew rate
Resistor footprint at BTST to adjust slew rate if needed.
Higher resistor value (slower slew rate) can adversely affect converter efficiency.
3.Use Snubber to reduce EMI
Snubber (resistor & capacitor) footprint at SW to control EMI source
Components must be placed closest to SW to be effective
4.Use EMI bead to reduce EMI
EMI Bead footprint at VBUS and PMID to suppress EMI
EMI beads selected must be able to handle high power with high impedance between 100MHz and 250MHz to effectively filter EMI at required FCC frequency range.
5.The load connection is also very important. An external wider and shorter wire may improve EMI performance.
Thanks,
Ning.