bq27510-G3 has two kind of Ra tables, Ra0 and Ra1.
After learning cycle, I think one of these Ra tables is updated, the other is default value.
On battery removable application,
Is there possibility that default Ra table is selected faultily?
If it is yes,
Should we clear IDSELEN bit if used battery is same type though battery is removable?
Which Ra table is selected when IDSELEN bit is 0, Ra0 or Ra1? In this case, is Ra0 always selected?
Or should we copy same Ra table value from Ra0 to Ra1?
Best Regards,
Kohei Sasaki