This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62130: Output voltage at light load

Part Number: TLV62130

Hi support team,

It is used with 12V input and 3.3V output.
However, when the load is light (probably a few mA), about 3.6V is output.
Do you know what caused it?

When a load current of about 15mA is applied, it stabilizes at 3.3V.

Regards,
Dice-K