Please provide more detail information (see below questions) for Reverse Direction function of BQ79606, such as example case, scenarios, docs, sample code.
Q1: Dose the Reverse Direction function can be performed without an auto-addressing ahead (ex: after a wakeup command)?
Q2: Does that mean whatever the break link between the two devices, the Reverse Direction function is able to re-connect all devices by the function performed?