Hi Team,
I am working with a customer who is planning to use TPS546D24ARVFR for a design stepping from 12V (10.8-13.2V range) to 0.72V @30A. How many 10uF 35V X5R 1210 ceramic input capacitors would you recommend using? We have a 2.2nF and 1uF cap for high frequency filtering but it would help to know how many other caps should be paralleled in addition to the bulk capacitance. Is the primary contributor to the number of paralleled caps to be below the max ESR which can be calculated in the DS (8.2.2.5 equation 24)? Any other factors? Thanks for your help!
Regards,
Garret