Hi team,
Could you tell me how to know input current in light load condition with PFM mode?
- I found that "7.5 Electrical Characteristics" says IQ-nonSW (Operating quiescent current (nonswitching)) is 36uAmax.
In addition, footnote(2) says "This is the current used by the device open loop. It does not represent the total input current of the system when in regulation".- Does nonswitching means only the duration which is shown in lower figure? So it is not total consumption current in PFM mode, is it correct?
- Which other current are needed for finding total input current?
- Does figure. 22 Efficiency could indicate total input current?
For example, 10mA output current, 5V output voltage, and 12V input voltage, then efficiency is about 82%.
This shows total input current is 25.4mA, is it correct?
If correct, could you tell me why this value is much different form IQ-nonSW?
Regards,
Ochi