When the voltage of the ultracapacitor is less than 2.1V, the output current is only 25mA. Is there any solution to make the capacitor charge according to the set current even when the voltage is less than 2.1V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When the voltage of the ultracapacitor is less than 2.1V, the output current is only 25mA. Is there any solution to make the capacitor charge according to the set current even when the voltage is less than 2.1V
Hi,
BQ24640 charges according to CC-CV charge profile without precharge current. If sensed battery voltage is < 2.1V then there should be no issue as is it can charge at fast charge from 0V battery.