Hi,
Here are the design requirements and configuration of the TPS61088 IC in my PCB
- Supply Source: 2 x Lithium Ion Batteries (in parallel)
- Output configuration: 7.5V and 2A
- Operating Mode: PWM
- Inductor used: Bao Cheng Elec BCIHP0718-1R0M (1uH) Saturation current: 11.5A
- EN pin is pulled high (4.1V)
I am testing the output capabilities of the TPS circuitry using 2 x 10 Ohms, 7 Watt load resistors connected in parallel to the output of the TPS61088 IC.
From the tests I have noticed when a single load resistor is connected to the output, the TPS IC is able to source the required current (~780mA) but when a second load resistor is added at the output in parallel, there is a >0.50V voltage drop. Here is the schematic diagram of the TPS60188 circuitry. The values in black are the ones that are soldered on the board.
Test notes,
LOAD: One 10 Ohm, 7W Load resistance
- Current consumption at output - 713mA
- Voltage at output when load is connected - 7.51V
- Voltage across VIN (C610) pin of TPS61088 IC when load is connected - 3.08V
- Voltage across VCC (C604) pin of TPS61088 IC when load is connected - 5.51V
LOAD: 2 x 10 Ohm, 7W Load resistance
- Current consumption at output - 1030mA
- Voltage at output when load is connected - 5.36V
- Voltage across VIN (C610) pin of TPS61088 IC when load is connected - 3.06V
- Voltage across VCC (C604) pin of TPS61088 IC when load is connected - 5.20V
UPDATE:
After going through a few posts about the TPS61088 IC, I reconfigured the output voltage of the TPS61088 IC to 5.98V (Changed R602 to 300K and R606 to 73K) and tried the load tests again.
But there still is a voltage drop at higher loads (>550mA)
LOAD: One 10 Ohm, 7W Load resistance
- Current consumption at output - 550mA
- Voltage at output when load is connected - 5.97V
- Voltage at VIN (C610) pin of TPS61088 IC when load is connected - 3.3V
- Voltage at VCC (C604) pin of TPS61088 IC when load is connected - 5.3V
LOAD: 2 x 10 Ohm, 7W Load resistance
- Current consumption at output - 1.042A
- Voltage at output when load is connected - 5.48V
- Voltage at VIN (C610) pin of TPS61088 IC when load is connected - 2.77V
- Voltage at VCC (C604) pin of TPS61088 IC when load is connected - 5.23V
Any help will be greatly appreciated. Thank you.
Regards,
Rutvik