Hello E2E team,
I want to test the behavior of our design using the TPS1H100A-Q1 high-side switch. Since I need to simulate the design with encrypted models, I have to use the PSpice model. Running the SLVMAI7A project in PSpice 17.4 gives me the output "ERROR(ORPSIM-15141): Less than 2 connections at node CL.". Adding an additional clamping resistor clears the error, but there is no CL current, and so there is no load current. Maybe it has something to do with CL been shown as an input pin? Interestingly, when using the .lib model with LTSpice, the TPS1H100A seems to work fine. Is there anything I can do to make the model work in PSpice?
Best Regards,
Niklas