Other Parts Discussed in Thread: TPS22918
My customer is using TPS22918-Q1 and complaining that they have a too-long 2ms delay time. According to their application(Vin=3.3V, Cct=1nF) I found the typical values of td=590us and tr=1680us from datasheet, whose sum is approximately 2.3ms. I confirmed with customer that they want the "delay time" (to 90% Vout) to be less than 250us.
I'd like to know whether we have a p2p part of TPS22918 with faster delay time and rise time? If customer decreases Cct, the tr will be shorter according to the formula and table in 8.3.3. What will be the td? The customer is using large Cout, will it cause the issue of inrush current?
Another question is about the definition of timing characteristics. Customer asked about the turn-on control logic. Why the starting point of ton and td is Von rising above 50%? According to the datasheet, the threshold voltage seems to be 1V? Why it isn't Von rising above 1V?
The customer would like to know the delay time of Von rising above 1V and Vout rising above 50% and 90% respectively. Do you have this data of the recommended part? Thanks