This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28600: New Transformer Design - 10V-30VDC with UCC28600 for SA-3-EE2005S-H10-11.0

Part Number: UCC28600

Dear Sir ,

We are using Texas device UCC28600D device in our power supply and require xmer specs as per following input.

 

Primary :- 

10V-30VDC : Start - pin 3 , End - pin 1

 

Secondaries :-

1)  5.6V @ 600mA : Start - pin 6 , End - pin 5  ( main winding)  

2)  12V @ 120mA : Start - pin 8, End - pin 7   

3)  12V @ 120mA : Start - pin 10, End - pin 9  

 

BOBBIN :- 10 pin EE2005S Horizontal.

 

Also mention primary inductance.

  • Hi Mahesh,

    It sounds like you have already worked out some of the details of the UCC28600 transformer design? If you have not yet worked through the calculations, I would recommend to start by downloading the UCC28600 Design Tool Calculator. TI does not manufacture custom magnetics/transformers/inductors. A quick web search will reveal there are many qualified magnetics vendors that can provide transformer samples from your spec.

    Regards,

    Steve