Other Parts Discussed in Thread: BQ7718
Hi Team,
In one of my customer application the maximum charger voltage is 10.5V and BQ29209 datasheet recommend maximum VDD voltage is 10V. Can 10.5V input damage the device since absolute maximum rating is 16V.
Can you plaese help suggesting 2cell device which can work on 10.5V max charger supply voltage and with over voltage protection of 4.2V.
Thanks in advance for the help and support.
Regards, Shinu Mathew.