I am using Ucc256402 for half bridge LLC converter, where Vhv = 150V.
I referred datasheet where it is mentioned that Vcc supply voltage range is Min: 13V, Nom: 15V, Max: 26V in recommended operating condition table.
But IC didn't work when I gave 24V at Vcc pin, then I came across another table which mentioned VCCStartSelf: min :25V, TYP: 26V, Max: 28V !!!!!!
So my question is if IC doesn't work below 26V ( which I observed so far) then what is the meaning of recommended operating condition ?
Regards,
Jitendra suthar