Part Number: TL2844B
Other Parts Discussed in Thread: UC2843A-Q1
Hi,
My customer is using TL2844BD8 but the temperature range of the TL2844-BD8 is limited to + 85 ° C, and I would need a version with an extended range of + 125 ° C, does it exist? If there is no SO-8 version with an extended temperature range, is there another similar integrated that can be right for me?
It should be used on inverter power board to supply the 24V.
Many Thanks,
Antonio