This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TPS61088: The variation of current limit point

Mastermind 37680 points

Replies: 1

Views: 58

Part Number: TPS61088

Hi,

Could you tell me about variation of current limit point?
The data sheet describes the current limit variation information of the specific condition.

However, customers want variation information other than 100kΩ.
Please tell me how to estimate the current value MIN and MAX obtained by the following calculation.

Best Regards,
Helen

Boost DC/DC Solution

  • Dear Sir,

    For the minimum value, it is: 

    Under PFM mode,
    Ilim=1190000/Rlim=yA typ, minimal Ilim=yA-1.3A;

    Under the PWM mode,
    Ilim=1190000/Rlim -1.6A=yA-1.6A , minimal Ilim=yA-1.6A-1.3A;

    For the maximum value, it is

    Under PFM mode,
    Ilim=1190000/Rlim+1.1A maximum

    Under the PWM mode,
    Ilim=1190000/Rlim -1.6A+1.1A maximum

    Best Regards,
    Helen

    Boost DC/DC Solution

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.