This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2002T: Suggest Charger circuit For BQ2002T

Part Number: BQ2002T
Other Parts Discussed in Thread: LM317

Hi All

Hope all are fine

BQ2002T how can we set chargine current or it has inbuilt fast charging means what is the charging rate ?

Either the charging current is adjustible or fixed 

My specifications 

Input : 5V 500mA  USB

Battery: 2 cells NImh 1.2V /800 mAh

Charging current expected : 0.5C 

Termination Style: Change in temperature /Cahnge in voltage 

Can you guys give me a better circuit or recommend an IC which meets above specs in TI