Other Parts Discussed in Thread: PMP7282
Hi Team,
A customer designed a LM5116 DC/DC converter with the following specifications.
Vin= 48VDC
Vout = 12VDC
Iout = 10A
The board was not able to produce 10A so he redesigned the schematic diagram based on PMP7282. I have checked the schematic diagram and the circuit seems okay. He would like to consult the values of the compensation network before he fabricate another board but due to confidentiality of his design we can't post it here in the forum.
Regards,
Danilo